Job Description
Job Title:  MATERIALS PLANNING SUPPORT V
Posting Start Date:  12/16/25
At TE, you will unleash your potential working with people from diverse backgrounds and industries to create a safer, sustainable and more connected world. 
Job Description: 

Job Overview

Plans, schedules, and monitors the movement of the materials through the production cycles and forecasts the material and labor requirements based on upcoming orders.

Job Requirements

  • Projecting revenues for assigned value streams, assisting with the capacity analysis and managing the scheduling plan in accordance with the inputs of the sales and operations department.
  • Coordinating with the sales function to provide lead times based on the schedule of the plant and meeting the timelines and metrics for the key stakeholders and customers.
  • Evaluating the cost and quality of the materials, collaborating with the production and engineering teams to determine the order date and quantity of the materials.
  • Monitoring the performance of the suppliers, suggesting inputs in the strategic sourcing of the goods, and assisting with the documentation to initiate the purchase.

What your background should look like

Typically requires more than 6 years of related work experience. Completion of an AA degree or equivalent is preferred. May be considered entry level for employees with Bachelor's degree in appropriate field or equivalent.

Competencies

Values: Integrity, Accountability, Inclusion, Innovation, Teamwork

Job Locations:

Suzhou, Jiangsu 215101
China

Posting City:  Suzhou
Job Country:  China
Travel Required:  10% to 25%
Requisition ID:  144632
Workplace Type: 
External Careers Page:  Manufacturing