Loading...
Share this Job
Apply now »

Programador Sénior - Eng. de Automação (m/f)

At TE, you will unleash your potential working with people from diverse backgrounds and industries to create a safer, sustainable and more connected world. 

Job Overview

TE Connectivity's Manufacturing Engineering Teams are process leaders for stamping, molding or assembly related topics, ensuring the processes are running at optimum levels for quality and output. They are experts in mold tooling, die tooling, machining, and assembly techniques, possessing extensive knowledge of the associated manufacturing processes which may include the optimization and standardization of stamping / molding / assembly or other processes within the manufacturing environment. Manufacturing Engineering Teams enable the TE business unit plants to reach TE Operating Advantage (TEOA) requirements, roll out Centers of Excellence (COE), Best Demonstrated Practices (BDP’s) and advise plants on tool and machine duplications / corrections / improvements. They design and develop manufacturing process and automation platforms and apply them for the realization of new product developments as well as optimization of existing products already in production. The Teams also support Product Development in the selection and optimization of tools for piece part production and the selection of the most suitable manufacturing concepts relative to planned manufacturing quantities, quality requirements and manufacturing location. They act as interface between engineering and production to ensure manufacturability of new designs and smooth production ramp up as well as support the research & development teams to produce sample manufacturing equipment, product samples and prototypes.

Responsabilidades & Background

Tarefas e/ou Responsabilidades 
 Projetar comandos de controlo para automação
 Projetar todo o circuito elétrico de máquinas
 Projetar o circuito pneumático de acordo com o projeto mecânico
 Programação de nível superior em automação (S7, ou outra plataforma em uso)
 Integrar uma equipa ME multi-disciplinar (Eng. de processo, Eng. de projeto Mecânico, e técnicos de montagem eletromecânica). 
 Coordenação técnica da equipa ME (em Go-Meetings) desde o arranque do projeto até ao FOT. Após o FOT, acompanhar e dar 
suporte à equipa durante a fase de debug. 
Tarefas detalhadas: 
 Investigar todos os dados relativos ao produto e ao processo para definir a tecnologia a aplicar 
 Avaliar e colaborar na elaboração do diagrama de movimentos 
 Efetuar os testes que necessários para determinar viabilidade da tecnologia na aplicação (Camaras, checkers, novo hardware 
etc) 
 Desenvolver conceitos tendo como base a cotação inicial do projeto, caderno de encargos, especificações etc.
 Executar os esquemas elétricos e pneumáticos em E-plan de acordo com as regras estandardizadas no departamento
 Programar os equipamentos de forma clara, baseado nas regras estandardizadas no departamento
 Manter os componentes atuais aplicando novos componentes quando necessário e corigindo componentes obsoletos
 Verificar a conformidade das ligações (terras, marcações, espessura dos condutores)
 Efetuar uma avaliação dos erros como forma de lições aprendidas
 Colaborar com o programador sénior na estandardização de novos itens
 Comentar o código de forma a poder ser interpretado por outros programadores 
 Fazer os manuais de instruções e de manutenção elétrica (nos casos em que esteja associado a manutenção programada)
 Efetuar “design reviews” com a equipa e os “coach” internos (seguindo o PIF)
 Efetuar “design reviews” com fornecedores externos.

Requisitos da Função 
Grau académico 
 Licenciatura ou Mestrado em Engenharia Eletrónica ou Mecatrónica 

Background
1 ano em eletrónica de automação
Mandatório: 
 Bons conhecimentos de eletricidade, eletrónica e automação 
 Bons Conhecimentos de informática 
 Boa capacidade de trabalho em equipa 
 Forte envolvimento, flexibilidade e resiliência 
 Boa capacidade de comunicação 
 Fluência em Inglês, falado e escrito 
Preferencial: 
 Conhecimentos da diretiva máquinas 
 Conhecimentos de programação em C++ S7 e Labview 
 Conhecimentos de eletrónica a nível de componente
 

Competencies

Values: Integrity, Accountability,Teamwork, Innovation
Location: 

EVORA, 07, PT, 7002-552

City:  EVORA
State:  07
Country/Region:  PT
Travel:  Less than 10%
Requisition ID:  68632
Alternative Locations: 
Function:  Engineering & Technology


Job Segment: Engineer, Machinist, Manufacturing Engineer, R&D Engineer, Engineering, Manufacturing, Automotive

Apply now »